cancel
Showing results for 
Search instead for 
Did you mean: 

How to set up MDK-ARM, cmsis, stlib 3.5.0 for 16Mhz HSE

sam239955
Associate II
Posted on December 07, 2011 at 00:25

Hi,

i want to know how to setup my stm32f103ze (HD) project correctly to 16mhz HSE. I build up a device with 16mhz NOT 8mhz. I want to use USB and USART too.

It would be nice to have a helping hand.

with regards

sam

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
sam239955
Associate II
Posted on December 07, 2011 at 01:52

the solution:

USE_STDPERIPH_DRIVER, STM32F10X_HD, HSE_VALUE=16000000

in keil as preprocessor variable

and set XTAL to 16.0

here is my init of rcc_clocks for my stm32f103zet6

/******************************************************************************/

/* SETUP.C: Setup Functions                                                     */

/* IMU200 16MHz HSE      72Mhz = 16Mhz/2*9                                    */

/******************************************************************************/

#include ''stm32f10x.h''                            /* STM32F10x Library Definitions      */

#include ''misc.h''

#include ''Setup.h''

extern volatile unsigned char  Clock1s;

extern volatile unsigned char  Clock100ms;

extern volatile unsigned long  TimeTick;

/* Variables */        

ErrorStatus HSEStartUpStatus;

GPIO_InitTypeDef  GPIO_InitStructure;

I2C_InitTypeDef  I2C_InitStructure;

SPI_InitTypeDef  SPI_InitStructure;

USART_InitTypeDef USART_InitStructure;

void SetupClock (void)

{

 /* SYSCLK, HCLK, PCLK2 and PCLK1 configuration -----------------------------*/   

     

  /* RCC system reset(for debug purpose) */

  RCC_DeInit();

  /* Enable HSE */

  RCC_HSEConfig(RCC_HSE_ON);

  /* Wait till HSE is ready */

  HSEStartUpStatus = RCC_WaitForHSEStartUp();

  if(HSEStartUpStatus == SUCCESS)

  {

    /* Enable Prefetch Buffer */

    FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable);

    /* Flash 2 wait state */

    FLASH_SetLatency(FLASH_Latency_2);

 

    /* HCLK = SYSCLK */

    RCC_HCLKConfig(RCC_SYSCLK_Div1);

 

    /* PCLK2 = HCLK */

    RCC_PCLK2Config(RCC_HCLK_Div1);

    /* PCLK1 = HCLK/2 */

    RCC_PCLK1Config(RCC_HCLK_Div2);

    /* On STICE the PLL output clock is fixed to 72 MHz */

    RCC_PLLConfig(RCC_PLLSource_HSE_Div2, RCC_PLLMul_9);

    /* Enable PLL */

    RCC_PLLCmd(ENABLE);

    /* Wait till PLL is ready */

    while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET)

    {

    }

    /* Select PLL as system clock source */

    RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);

    /* Wait till PLL is used as system clock source */

    while(RCC_GetSYSCLKSource() != 0x08)

    {

    }

 }

/* set SysTick */

    SysTick_Config(72*1000*10);

/* Enable GPIO Clocks */

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE);

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE);

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOD, ENABLE);

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOE, ENABLE);

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOF, ENABLE);

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE);    

}