Skip to main content
JAltu.1
Associate II
January 20, 2025
Solved

How to set RTC secure mode STM32U5 Series

  • January 20, 2025
  • 1 reply
  • 853 views

I would like to use the WKUP 6 (RTC_WUT_S) to wake up from Standby mode. I am already using WKUP 7 with a pin so I need the RTC to be in safe mode.

What would be the best way?

Best answer by STea

Hello @JAltu.1 ,

You can't add Trustzone to an existing non-Trustzone application. you will have to start a new project with Trustzone enabled in order to have the isolation and security features that it offers with the secure and non-secure projects.

Regards

1 reply

ST Employee
January 20, 2025

Hello @JAltu.1 ,

I don't get you exact request what do you mean by saying "RTC to be in safe mode".

are you working with trustzone enabled?
if yes then working with RTC in a safe way should be done by setting WUTSEC bit in control register 

When WUTSEC is set:
– RTC_WUTR register, plus WUTE, WUTIE and WUCKSEL control bits in the
RTC_CR, CWUTF in the RTC_SCR, WUTF in RTC_SR, and WUTMF in
RTC_SMISR can be read and written only in secure mode.
– WUTPRIV in the RTC_PRIVCFGR can be written only in secure mode
please refer to RM0456 section 63.3.4 RTC secure protection modes for more details. 
Regards

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JAltu.1
JAltu.1Author
Associate II
January 21, 2025

Hi @STea ,

Trustzone is disabled. I have seen it can be enabled creating a new project.

But how can I do it in a existing project?

Regards

STeaBest answer
ST Employee
January 21, 2025

Hello @JAltu.1 ,

You can't add Trustzone to an existing non-Trustzone application. you will have to start a new project with Trustzone enabled in order to have the isolation and security features that it offers with the secure and non-secure projects.

Regards

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.