Skip to main content
antonius
Associate III
April 26, 2015
Question

How to init GPIO on CubeMX generated code ?

  • April 26, 2015
  • 1 reply
  • 635 views
Posted on April 26, 2015 at 11:42

Guys,

I have generated a code for Keil from CubeMx but I can't initialize GPIO, I can see a code in main.c below....anyone knows how to initialize GPIO,reset and set a bit on it at CubeMx generated code ?? I used LwIP,USB and RTOS and FatFS...

HAL_GPIO_Init(GPIOE, GPIO_CR_CNF_GP_OUTPUT_PP );
/* USER CODE BEGIN 5 */
/* Infinite loop */
for(;;)
{
HAL_GPIO_WritePin(GPIOE,5,0);
osDelay(2000000);
HAL_GPIO_WritePin(GPIOE,5,1);
osDelay(2000000);
osDelay(1);
}
/* USER CODE END 5 */

complete main.c :

/**
******************************************************************************
* File Name : main.c
* Date : 26/04/2015 05:25:33
* Description : Main program body
******************************************************************************
*
* COPYRIGHT(c) 2015 STMicroelectronics
*
* Redistribution and use in source and binary forms, with or without modification,
* are permitted provided that the following conditions are met:
* 1. Redistributions of source code must retain the above copyright notice,
* this list of conditions and the following disclaimer.
* 2. Redistributions in binary form must reproduce the above copyright notice,
* this list of conditions and the following disclaimer in the documentation
* and/or other materials provided with the distribution.
* 3. Neither the name of STMicroelectronics nor the names of its contributors
* may be used to endorse or promote products derived from this software
* without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS ''AS IS''
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
* IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
* DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE
* FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL
* DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
* SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER
* CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
* OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
******************************************************************************
*/
/* Includes ------------------------------------------------------------------*/
#include ''stm32f1xx_hal.h''
#include ''cmsis_os.h''
#include ''fatfs.h''
#include ''lwip.h''
#include ''usb_host.h''
//Define LED port begin
/* led connected to a gpio pin */
#define LED1_PIN GPIO_Pin_0
#define LED1_PORT GPIOB
#define LED2_PIN GPIO_Pin_3
#define LED2_PORT GPIOC
//#define LED3_PIN GPIO_Pin_0
//#define LED3_PORT GPIOA
//#define LED4_PIN GPIO_Pin_0
//#define LED4_PORT GPIOE
#define LED3_PIN GPIO_Pin_5
#define LED3_PORT GPIOE
#define LED4_PIN GPIO_Pin_6
#define LED4_PORT GPIOE
#define LED1_D_PIN GPIO_Pin_5
#define LED1_D_PORT GPIOD
//Define LED port END
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private variables ---------------------------------------------------------*/
USART_HandleTypeDef husart2;
osThreadId defaultTaskHandle;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_Init(void);
void StartDefaultTask(void const * argument);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART2_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* USER CODE BEGIN RTOS_MUTEX */
/* add mutexes, ... */
/* USER CODE END RTOS_MUTEX */
/* USER CODE BEGIN RTOS_SEMAPHORES */
/* add semaphores, ... */
/* USER CODE END RTOS_SEMAPHORES */
/* USER CODE BEGIN RTOS_TIMERS */
/* start timers, add new ones, ... */
/* USER CODE END RTOS_TIMERS */
/* Create the thread(s) */
/* definition and creation of defaultTask */
osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 128);
defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);
/* USER CODE BEGIN RTOS_THREADS */
/* add threads, ... */
/* USER CODE END RTOS_THREADS */
/* USER CODE BEGIN RTOS_QUEUES */
/* add queues, ... */
/* USER CODE END RTOS_QUEUES */
/* Start scheduler */
osKernelStart();
/* We should never get here as control is now taken by the scheduler */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/** System Clock Configuration
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_PeriphCLKInitTypeDef PeriphClkInit;
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1;
RCC_OscInitStruct.Prediv1Source = RCC_PREDIV1_SOURCE_HSE;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL6;
RCC_OscInitStruct.PLL2.PLL2State = RCC_PLL_NONE;
HAL_RCC_OscConfig(&RCC_OscInitStruct);
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1);
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USB;
PeriphClkInit.UsbClockSelection = RCC_USBPLLCLK_DIV2;
HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit);
__HAL_RCC_AFIO_CLK_ENABLE();
}
/* USART2 init function */
void MX_USART2_Init(void)
{
husart2.Instance = USART2;
husart2.Init.BaudRate = 115200;
husart2.Init.WordLength = USART_WORDLENGTH_8B;
husart2.Init.StopBits = USART_STOPBITS_1;
husart2.Init.Parity = USART_PARITY_NONE;
husart2.Init.Mode = USART_MODE_TX_RX;
husart2.Init.CLKPolarity = USART_POLARITY_LOW;
husart2.Init.CLKPhase = USART_PHASE_1EDGE;
husart2.Init.CLKLastBit = USART_LASTBIT_DISABLE;
HAL_USART_Init(&husart2);
}
/** Configure pins as 
* Analog 
* Input 
* Output
* EVENT_OUT
* EXTI
*/
void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOE_CLK_ENABLE();
//PORT E ALL PINS OUT
/*Configure GPIO pins : PC13 PC14 PC15 PC0 
PC1 PC2 PC3 PC4 
PC5 PC6 PC7 PC8 
PC9 PC10 PC11 PC12 */
GPIO_InitStruct.Pin = GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15|GPIO_PIN_0 
|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_4 
|GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_8 
|GPIO_PIN_9|GPIO_PIN_10|GPIO_PIN_11|GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
//GPIO_InitStruct.Pull = GPIO_PULLUP;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
/*Configure GPIO pins : PD8 PD9 PD10 PD11 
PD12 PD13 PD14 PD15 
PD0 PD1 PD2 PD3 
PD4 PD5 PD6 PD7 */
GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15; 
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct); 
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/* StartDefaultTask function */
void StartDefaultTask(void const * argument)
{
/* init code for FATFS */
MX_FATFS_Init();
/* init code for LWIP */
MX_LWIP_Init();
/* init code for USB_HOST */
MX_USB_HOST_Init();
/* init code for GPIO */ 
// MX_GPIO_Init();
/* USER CODE BEGIN 5 */
/* Infinite loop */
for(;;)
{
HAL_GPIO_WritePin(GPIOE,GPIO_PIN_5,GPIO_PIN_RESET);
osDelay(200);
HAL_GPIO_WritePin(GPIOE,GPIO_PIN_5,GPIO_PIN_SET);
osDelay(200);
osDelay(1);
}
/* USER CODE END 5 */ 
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */
/* USER CODE END 6 */
}
#endif
/**
* @}
*/ 
/**
* @}
*/ 
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

thanks
    This topic has been closed for replies.

    1 reply

    Amel NASRI
    ST Technical Moderator
    April 29, 2015
    Posted on April 29, 2015 at 10:41

    Hi h.rick,

    The purpose of CubeMX is to provide initialization code for GPIOs as well as other used peripherals.

    Before reviewing code you are providing, please let us know what are you facing as issue and what are you expecting as GPIO initialization.

    -Mayla-

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.