2021-03-06 6:46 AM
Hi, I am running an application on the STM32L562-DK. The performance of the application is lower than anticipated. I started investigating what could be causing the performance issues. I found some example projects that had hal function calls to enable icache. I started to port over the functions to enable icache to my project and experienced a lot of fan out in regards to all the files and dependencies associated with adding the hal functional calls. I also notices that there is an .ioc that contains cache configurations. My current project does not have an associated .ioc and not sure how to add one and if it is required.
Is there any documentation on how to integrate cache functionality into an MCUExpresso project?
-Steve