Skip to main content
David Krcmarik
Associate
July 30, 2018
Question

How to configure SPI1 in Nucleo L476RG in SPI_DATASIZE_8BIT mode

  • July 30, 2018
  • 3 replies
  • 1601 views

Hello,

please can I ask how to configure SPI1 in Nucleo L476RG? I have configured SPI interface using CubeMX and then I have checked the functionality using osciloscope. When I want to send 1 byte (8 bits) CLK signal generated has 16 pulses instead of 8 pulses. My configuration of SPI is:

static void MX_SPI1_Init(void) {

/* SPI1 parameter configuration*/

hspi1.Instance = SPI1;

hspi1.Init.Mode = SPI_MODE_MASTER;

hspi1.Init.Direction = SPI_DIRECTION_2LINES;

hspi1.Init.DataSize = SPI_DATASIZE_8BIT;

hspi1.Init.CLKPolarity = SPI_POLARITY_HIGH;

hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;

hspi1.Init.NSS = SPI_NSS_SOFT;

hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_16;

hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;

hspi1.Init.TIMode = SPI_TIMODE_DISABLE;

hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;

hspi1.Init.CRCPolynomial = 7;

hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;

hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;

if (HAL_SPI_Init(&hspi1) != HAL_OK) {

_Error_Handler(__FILE__, __LINE__);

}

}

I have checked also the registers in HAL_SPI_Init and everything seems fine. Basically when I choose some hspi1.Init.DataSize the number of CLK pulses is always doubled. It seems to me it could be some problem in HAL. Please can you help me how to configure SPI in a such way I would be able to use it for hspi1.Init.DataSize = SPI_DATASIZE_8BIT (it means 8 CLK pulses for each byte)? Attached is a screenshot from osciloscope and program.

David Krcmarik

    This topic has been closed for replies.

    3 replies

    David Krcmarik
    Associate
    July 30, 2018

    I have forget this function definition for code:

    int32_t SPI_WriteReadByte(uint8_t data)

    {

    while (!__HAL_SPI_GET_FLAG(&hspi1, SPI_FLAG_TXE));

    hspi1.Instance->DR = data;

    while (!__HAL_SPI_GET_FLAG(&hspi1, SPI_FLAG_RXNE));

    return (int32_t)hspi1.Instance->DR;

    }

    Tesla DeLorean
    Guru
    July 30, 2018

    Watch the width of the write to DR lest it stuff 16-bits worth of data into the FIFO

    *((volatile uint8_t *)&hspi1.Instance->DR) = data;

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    David Krcmarik
    Associate
    August 1, 2018

    Thanks this works.