Skip to main content
Visitor II
December 23, 2024
Question

How to Change Sampling Rate for LSM6DSO32G in Samsung Android Kernel?

  • December 23, 2024
  • 1 reply
  • 600 views

I am currently working on modifying the sampling rate for the LSM6DSO32G IMU sensor in a Samsung Android kernel. After reviewing the device tree and sensor driver files, I noticed that certain parameters like odr (output data rate) seem to control the sampling rate. However, I am not sure of the exact steps to apply these changes and ensure that the modified sampling rate is reflected correctly in the system.

Here are my specific questions:

  1. Which files in the Samsung Android kernel should I modify to change the sampling rate for the LSM6DSO32G?
  2. Do I need to make changes in both the driver source code and the device tree, or is one sufficient?
  3. Is there a way to dynamically update the sampling rate (e.g., via sysfs or a similar interface) without rebuilding the kernel?
  4. Are there any specific steps or precautions I should take to test and validate the changes?

Any guidance, code examples, or references to related documentation would be greatly appreciated!

Thank you in advance for your help.

Best regards,

This topic has been closed for replies.

1 reply

Andrew Neil
Super User
December 23, 2024

You need to go to a suitable (Samsung) Android developer's forum - none of this has anything to do with ST.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.