Skip to main content
Vu.Andy
Associate III
November 3, 2017
Question

How should I set my ''heap'' and ''stack'' size

  • November 3, 2017
  • 7 replies
  • 5684 views
Posted on November 03, 2017 at 18:04

After compiling the codes, my code size is:

Program Size: Code=20140 RO-data=316 RW-data=540 ZI-data=2412 

Based on this information, how should I set my 'heap' and 'stack' size? 

My first question is the 'heap' and 'stack' size is for Per Function call?  Or is it for the entire program?

For example, if all my global variables are added up to, for example, 700 bytes total, then do I need to

set my 'heap' size to be at least 700 bytes?  What would happen if I set heap size less than 700 bytes?

Of course each function call will have its own variables, and each function will call other functions so the stack size may not be known in advance.  Will the uProcessor crash if the allocated 'stack' size in the .S file is less than needed during runtime?

So I guess my question is how would you determine heap and stack size?

Thanks.<

    This topic has been closed for replies.

    7 replies

    Tesla DeLorean
    Guru
    November 3, 2017
    Posted on November 03, 2017 at 18:24

    Global variables don't use the heap.

    Local/auto variables use the stack (or registers as the compile feels appropriate), and their usage and your call depth will dictate how large the stack needs to be.

    If you have something like

    void foo(void)

    {

      uint8_t bar[512];

    ..

    }

    You're going to need a stack with over 512 bytes in it.

    You can do some static analysis of your own code.

    You can look at the .HTML file Keil's Linker generates with respect to stack utilization and call trees.

    You can do dynamic analysis by filling the stack with a data pattern you recognize, and then look at how deep into the stack you get via the debugger, and a memory view place over the stack area.

    You can have a routine that probes the stack to determine a maximal depth, and review that periodically.

    The heap is going to be used by malloc() or new operations, malloc will return a NULL if it is full, you should aggressively check for this in your code.

    You can walk the heap to see how much space remains, and the size of the largest contiguous piece.

    The heap can have issues with fragmentation and resource leaks, you can wrap the malloc/free routines to monitor or instrument this.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Vu.Andy
    Vu.AndyAuthor
    Associate III
    November 7, 2017
    Posted on November 07, 2017 at 18:39

    Thanks for the information.  I looked in the .html to find the function call with the maximum stack size and I guess I can approximate the stack size.

    Is there a way to use the debugger to look at the stack size dynamically?

    Thanks.

    Tesla DeLorean
    Guru
    November 7, 2017
    Posted on November 07, 2017 at 19:03

    '

    You can do dynamic analysis by filling the stack with a data pattern you recognize, and then look at how deep into the stack you get via the debugger, and a memory view place over the stack area.

    '
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    S.Ma
    Principal
    November 3, 2017
    Posted on November 03, 2017 at 18:59

    Usually a linker will issue a MAP file and try to estimate recursively the stack depth for all things pointed from the interrupt vector table, from reset, from interrupts. This gives a rough idea of the stack size. If you use function pointers and/or malloc, the linker will be unable to give you a reliable figure, you'll have to top the number up.

    If using an RTOS, things get worse as in this case you probably need a stack per task...

    If short in RAM, check if you can use a buffer for multiple purpose at different time using 'union'

    If using floats/double, check if you can use a fractional integer.

    Look into the map file for each object file the needs in stack and global variable ram area.

    JulienD
    Associate III
    May 7, 2018
    Posted on May 07, 2018 at 18:14

    Hello,

    Rather old thread but I've just found this interesting page:

    https://community.arm.com/processors/b/blog/posts/how-much-stack-memory-do-i-need-for-my-arm-cortex--m-applications

     

    Julien