Skip to main content
arnold_w
Senior II
January 19, 2018
Question

How do I get the frequency of a timer in STM32F769I?

  • January 19, 2018
  • 5 replies
  • 8674 views
Posted on January 19, 2018 at 13:38

I am working with the STM32F7691I-EVAL board and I would like to determine the frequency of any given timer:

GET_TIMER_FREQ(TIMx)

The macro/function should be able to determine the frequency regardless of which clock the microcontroller is running from. Of course it is fully acceptable to do it 2 steps, first determine the clock source and then determine the resulting frequency for a particular timer. I have gone through the HAL-files, but I am unable to find such macros/functions. Can someone please help me?

    This topic has been closed for replies.

    5 replies

    Tesla DeLorean
    Guru
    January 19, 2018
    Posted on January 19, 2018 at 14:24

    The macro (or function) would need to know which APB a particular timer is on, and then check the divisor. I all except the DIV1 case the TIMCLK is source one divider tap earlier (ie *2)

    printf('APB1=%d\n', HAL_RCC_GetPCLK1Freq());

    printf('APB2=%d\n', HAL_RCC_GetPCLK2Freq());

    Review code in these functions

    For systems you know the configuration the computation for TIMxCLK can use SystemCoreClock

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    arnold_w
    arnold_wAuthor
    Senior II
    January 19, 2018
    Posted on January 19, 2018 at 14:45

    Where do I find out which timers are connected to which PCLKx? Is the same as STM32F4 (2: TIM1

    TIM8

    TIM9

    TIM10

    TIM11, and the rest are 1)?

    Tesla DeLorean
    Guru
    January 19, 2018
    Posted on January 19, 2018 at 16:56

    There is a bus diagram in the Data Sheet, APBxENR registers in the Reference Manual, and the ♯ include should associate the APB1 and APB2 clock enables for the various timers.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Associate III
    October 27, 2023

    The address of the timer determines which Bus it is on. I created below code which does the trick:

     

    RCC_ClkInitTypeDef clkConfig;

    uint32_t latency;

    uint32_t clockHz;

     

    ::HAL_RCC_GetClockConfig(&clkConfig, &latency);

     

    //= The address of the timer register determines which bus it is located on

    if ((uint32_t)peripheralReg >= APB2PERIPH_BASE)

    {

    clockHz = ::HAL_RCC_GetPCLK2Freq();

     

    if (clkConfig.APB2CLKDivider != RCC_HCLK_DIV1)

    {

    clockHz *= 2;

    }

    }

    else if ((uint32_t)peripheralReg >= APB1PERIPH_BASE)

    {

    clockHz = ::HAL_RCC_GetPCLK1Freq();

     

    if (clkConfig.APB1CLKDivider != RCC_HCLK_DIV1)

    {

    clockHz *= 2;

    }

    }

    Associate III
    October 28, 2023

    Additional to my previous post. What I forget to mention is that (uint32_t)peripheralReg is part of my extensive C++ library built on top of the HAL layer.

    This code is a reference to the Timer instance (TIM_TypeDef* Instance) in TIM_HandleTypeDef