cancel
Showing results for 
Search instead for 
Did you mean: 

Hi ST community, I would like to use CH340G USB UART converter for programming STM32F446RE Microcontroller. How can I do this? Any advice or idea about this? Thx a lot. :)

AElma.1
Associate II

Normally I use ST-link for programming. But I can not see data in serial port on computer. I use TMS,TCK,RST pins for programming. I would like to solve this issue for my new design. Could help me please? What I need to learn exactly ?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Review App Note AN2606 to understand the supported mode and pins for the ROM based System Loader

To program via a COM port / UART you could use the STM32 Cube Programmer application in UART/COM mode.

You'd enter the System Loader on the F446 by pulling the BOOT0 pin HIGH and reseting the device.

The protocol is described in other App Notes, AN3155 as I recall.

https://www.st.com/resource/en/application_note/cd00167594-stm32-microcontroller-system-memory-boot-mode-stmicroelectronics.pdf

https://www.st.com/resource/en/application_note/cd00264342-usart-protocol-used-in-the-stm32-bootloader-stmicroelectronics.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Peter BENSCH
ST Employee

You can use the STM32CubeProgrammer together with the correct settings for the boot sector which can be found in the AN2606, section 34 and table 2. For the STM32F446 the pattern is 1: Boot0 (pin) = 1 and Boot1 (pin) = 0.

After a reset, the STM32CubeProgrammer should be able to program via the USB-UART converter.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.