Skip to main content
oe_it
Associate III
September 9, 2009
Question

hi-speed UART

  • September 9, 2009
  • 2 replies
  • 716 views
Posted on September 09, 2009 at 13:57

hi-speed UART

    This topic has been closed for replies.

    2 replies

    picguy
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:23

    STM32 UARTs use the divide by 16 approach. Thus with a 72 MHz processor clock (I used an 8 MHz xtal) UART1 can run at 4.5 Mbaud. (About 25% of what I wanted. But that’s not your issue.) You need a 16*250 KHz = 4 MHz input to the UART.

    Unless you have power issues assume you are running with a 72 MHz processor clock. Look at the clock tree in general and UART1 frequency source in particular. Get at close as you can to 4 MHz. If you can not get close enough you may need to use another xtal. But check with your hardware people. Non-standard frequencies may be hard to obtain and therefore expensive.

    oe_it
    oe_itAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:23

    I need a hi-spped UART, running at 250kbaud. Do anyone have any suggestions?

    I suppose it would be possible to alter the X-tal and make the CPU run at a frequency that can be devided to get the correct baudrate.

    [ This message was edited by: oe on 09-09-2009 14:52 ]