Skip to main content
AAAZO.1
Associate
May 3, 2022
Question

USART1 doesn't communicate using HSE; worked with HSI

  • May 3, 2022
  • 2 replies
  • 866 views

Hello, I am new to the ST platform.

I actually work with a nucleo144, and i was trying to work with bluetooth hc-06, the problem is that USART1 doesn't communicate with the board when I use HSE in the clock configuration, but it worked when I use HSI

In my project I can't use HSI, do you have any suggestions please ?

 

 

This topic has been closed for replies.

2 replies

Peter BENSCH
ST Technical Moderator
May 3, 2022

Welcome, @AAAZO.1​, to the community!

The HSE can only be used if:

  • either an external frequency is fed in (bypass mode)
  • or a crystal and the associated passive components (capacitors, depending on the board also 0-ohm resistors) are fitted. 

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Nikita91
Lead II
May 3, 2022

On a Nucleo board the HSE clock can come from the STLINK, if it is not populated with a crystal.

But you have to consult the schematics of the board, on some Nucleo there is a solder bridge to add for this functionality.