Skip to main content
Associate III
April 10, 2023
Question

HAL_OSPI_Transmit_DMA not working for NbData > 0xFFFF .

  • April 10, 2023
  • 2 replies
  • 2264 views

Step to reproduce :

In cubeMX:

Select NucleoU575ZI.

Clean all pin

Set OCTOSPI to QSPI (see code below)

Configure GPDMA (see code below)

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2023 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "gpdma.h"
#include "octospi.h"
#include "gpio.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
 
/* USER CODE END Includes */
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
 
/* USER CODE END PTD */
 
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
 
/* USER CODE END PD */
 
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
 
/* USER CODE END PM */
 
/* Private variables ---------------------------------------------------------*/
 
/* USER CODE BEGIN PV */
uint8_t framebuffer_16bsize[65535]; //0xffff
uint8_t bigger_framebuffer[65536]; //0xffff
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void SystemPower_Config(void);
/* USER CODE BEGIN PFP */
 
void qspi_send_data(uint8_t * framebuffer, uint32_t size);
 
/* USER CODE END PFP */
 
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
 
/* USER CODE END 0 */
 
/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* Configure the System Power */
 SystemPower_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_GPDMA1_Init();
 MX_OCTOSPI1_Init();
 /* USER CODE BEGIN 2 */
 
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 
	 qspi_send_data(framebuffer_16bsize, sizeof(framebuffer_16bsize));
	 qspi_send_data(bigger_framebuffer, sizeof(bigger_framebuffer));
	 HAL_Delay(50);
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}
 
/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 /** Configure the main internal regulator output voltage
 */
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE4) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;
 RCC_OscInitStruct.MSIState = RCC_MSI_ON;
 RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_4;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_PCLK3;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
 {
 Error_Handler();
 }
}
 
/**
 * @brief Power Configuration
 * @retval None
 */
static void SystemPower_Config(void)
{
 
 /*
 * Switch to SMPS regulator instead of LDO
 */
 if (HAL_PWREx_ConfigSupply(PWR_SMPS_SUPPLY) != HAL_OK)
 {
 Error_Handler();
 }
/* USER CODE BEGIN PWR */
/* USER CODE END PWR */
}
 
/* USER CODE BEGIN 4 */
 
void qspi_send_data(uint8_t * framebuffer, uint32_t size)
{
	 OSPI_RegularCmdTypeDef sCommand = {0};
	 sCommand.OperationType = HAL_OSPI_OPTYPE_COMMON_CFG;
 
	 sCommand.Instruction = 0x32;
	 sCommand.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE;
	 sCommand.InstructionSize = HAL_OSPI_INSTRUCTION_8_BITS;
 
	 sCommand.Address = 0x2C << 8;
	 sCommand.AddressMode = HAL_OSPI_ADDRESS_1_LINE;
	 sCommand.AddressSize = HAL_OSPI_ADDRESS_24_BITS;
 
	 sCommand.AlternateBytesMode = HAL_OSPI_ALTERNATE_BYTES_NONE;
 
	 sCommand.DataMode = HAL_OSPI_DATA_4_LINES;
	 sCommand.NbData = size;
 
 
	 sCommand.SIOOMode = HAL_OSPI_SIOO_INST_ONLY_FIRST_CMD;
 
	 sCommand.DummyCycles = 0;
 
	 HAL_OSPI_Command(&hospi1, &sCommand, 1000);
//	 error = HAL_OSPI_Transmit(&hospi1, (uint8_t *) framebuffer, 5000);
 
	 HAL_OSPI_Transmit_DMA(&hospi1, (uint8_t *) framebuffer);
 
	 while (HAL_OSPI_GetState(&hospi1) != HAL_OSPI_STATE_READY){};
 
 
 
 
}
 
/* USER CODE END 4 */
 
/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}
 
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @param file: pointer to the source file name
 * @param line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

the "qspi_send_data(framebuffer_16bsize, sizeof(framebuffer_16bsize));" works perfectly as expected.

But the "qspi_send_data(bigger_framebuffer, sizeof(bigger_framebuffer))"; does not works and even stay in infinite loop with larger data.

The thing is : everywhere in hal doc and code the size is 32b and therefore should not be limited to 16b.

Regards

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
April 16, 2023

The DMA transfer counter register is 16-bit wide. It's a hardware limitation.

It doesn't have to count byte transfers. More data can go over in half-word or word forms.

For DMA units supporting double buffers there can be two separate or contiguous regions described.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
BerthaAuthor
Associate III
April 16, 2023

Dear Tesla DeLorean,

Thanks for your answer, maybe ST should modify function prototype to 16b.

Going to word forms will allow me to send 4*0xffff datas = 262 140 which is not enough.. I need 368*448*2 B = 329728 B.

I am sorry I am not sure to understand your last point, is this could be a solution to my issue ?

Or I should try something else ?

Regards