Skip to main content
Associate III
Jan 8, 2025 9:22 AM UTC
Question

Failed to inerface (4 and 8 GB) pendrive to STM32H747

 

Dear Community,

 

I am currently working on interfacing of USB (pen-drive) in FS mode with STM32H747BIT6.

I have observed that  during the enumeration process of pen-drive it is failing  to proceed at the function

USBH_HandleControl --> case CTRL_SETUP_WAIT: --> USBH_LL_GetURBState -->HAL_HCD_HC_GetURBState -->

hhcd->hc[chnum].urb_state is not changing to URB_DONE and continues to show URB_NOTREADY.

As the interrupt is not getting triggered for FS.

Is there any i can find if the problem subsides in Hardware or USB driver side.

Attaching schematic part for the reference.

Thanking in advance.

Regards

This topic has been closed for replies.

4 replies

Andrew Neil
Super User
Jan 8, 2025 9:29 AM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tesla DeLorean
Guru
Jan 8, 2025 9:41 AM UTC

No useful information presented. 

Instrument the USB interaction at first connection.

Show file system interaction at a block level.

Make sure it can read the MBR and BPB from the media and review what's happening differently between working and non-working cases.

Instrument error and status messages.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
RushaliAuthor
Associate III
Jan 9, 2025 11:17 AM UTC

@Andrew Neil

I have updated my query. Awaiting for the solution .

 

ST Technical Moderator
Feb 11, 2025 4:48 PM UTC

Hi @Rushali 

Could you explain why you use ULPI interface while operating in FS mode only?

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL