Skip to main content
izua
Associate III
September 27, 2010
Question

Exporting flash files from atollic

  • September 27, 2010
  • 13 replies
  • 2540 views
Posted on September 27, 2010 at 18:53

Is it possible to export flash files from atollic TrueStudio using a separate tool rather than the stock ''flash converter - not included with the lite version'' ?

    This topic has been closed for replies.

    13 replies

    Andrew Neil
    Super User
    October 25, 2010
    Posted on October 25, 2010 at 08:08

    ''I would have much preferred the tool chain to have done this, and perhaps have a code size limit for the demo/eval. Instead it removed things like projects...''

    And has also, apparently, been crippled to make it impossible to use printf !!

    They do seem to have gone out of their way to make this as unusable as possible...?

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    sjo2
    Visitor II
    October 27, 2010
    Posted on October 27, 2010 at 13:37

    see this thread as all are a just simple tweak away.

    https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Program%20chip%20using%20st-link%20in%20Atollic%20IDE

    Cheers

    Spen

    Tesla DeLorean
    Guru
    October 27, 2010
    Posted on October 27, 2010 at 14:52

    see this thread as all are a just simple tweak away.

     

     

    Yes, there is a link to that a couple of posts up. Came up with a quick Google around the topic.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..