ETM Trace on STM32L486QG
I want to do ETM trace on STM32L486QG.
When I look at my trace probe: I see I have to connect 5 pins TClock, T0,T1,T2,T3.
I am look at which pins to connect to on the processor. I found this document
https://www.st.com/resource/en/datasheet/stm32l486qg.pdf
on page 67, it looks like PE02, PE03, PE04, PE05 are used for TClock, T0,T1,T2,T3 respectively.
But in the same page, it looks like there are alternative use for the pins like FMC.
if we are already using these pins for other function like FMC , can we still use these pins for ETM tracing?
If not, can we assign other pins for that purpose?