Error in AN2867 regarding oscillator choice?
Hello,
I think I found an error in the AN2867 and just wanted to confirm it, before we hack around in hardware.
We use an H7 with an external LSE. Fate landed us on the ABRACON ABS05-32.768kHz with 12.5pF. According to AN2867 it is suitable for the H7 and many others.
Due to problems with the clock (which are not surprising NOW) I digged deeper into it and the H7 with LSE max drive is only suitable for a maximum critical crystal gain of 2.7, with the Abracon having a gain of 2.90612.
And, in fact, all other oscillator with a gain of >2.7 are only compatible with the F0 and F3.
So, am I on the right track with this being an error in the application note?
Best wishes
Christoph