cancel
Showing results for 
Search instead for 
Did you mean: 

Encoder mode using CHN instead of CH

kmce
Associate

Currently, I try to use an quadrature encoder connected on pins PC12, PC11 and PC10. All these pins have in common that they all can use Timer 8, for channels CHN1, CHN2 and CHN3. When I try to configure Timer 8 in Encoder mode; I can't select the CHN channels. Is there a way to use these pins as input for the encoder?

 

kmce_0-1718955733833.png

 

 

 

0 REPLIES 0