Skip to main content
sittingduck03
Visitor II
November 17, 2016
Question

DMA and RCC Low Power Enable bits (LPENR)

  • November 17, 2016
  • 0 replies
  • 592 views
Posted on November 17, 2016 at 20:02

I'm on an STM32F4 and using an RTOS.  I put the MCU to sleep whenever the scheduler has nothing to do using the WFI instruction.  

I'm using DMA1 with i2S and a USART.  I want to disable the DMA1 clock using the 

RCC_AHB1LPENR_DMA1LPEN bit which means the clock is disabled when the mcu is asleep.  The problem is that sometimes the UART doesn't

function

 when

RCC_AHB1LPENR_DMA1LPEN=0 even though the MCU is awake.  The UART is never able to complete it's transmission.  

Does anyone have any advice on how to use the 

RCC_AHB1LPENR_DMA1LPEN bit? Resetting it adds about an hour to battery life so I don't want to just leave it set all the time.

Thanks  

#sleep #wfi #rcc #ahb1lpenr
This topic has been closed for replies.