Associate
May 19, 2015
Question
DIY STM32F429 Evaluation Board
- May 19, 2015
- 3 replies
- 1436 views
Posted on May 19, 2015 at 09:31
hello,
i would like to introduce my self-made Evaluation Board for a STM32F429IGT6 (176 Pin LQFP) pictures are attached it's a 4 Layer 100mm x 50mm Board with onboard : 256MBit SDRAM 512kBit I2C-EEprom 16MBit SPI-Flash CAN-Transceiver FTDI-UART-Interface Mini-USB for USB-OTG Micro-SD-Card Connector Six Status LEDs And 2,54mm Header for many GPIOs and a 24bit TFT-Connector (a second board for interfacing a 4,3 inch TFT is following) here a link to my projectpage with further informations (only in german) Uwe #stm32f429