Associate III
July 16, 2024
Question
CUBEMx stucks when generating code
- July 16, 2024
- 2 replies
- 1227 views
hello!
I start this post because i have created a new project with CUBEMX 6.12.0 and i am having some issues.
When I generate code without THREAD X activated, the generation is completed without any error. However, when I add the thread X option (see .ioc file), the generation process gets stuck in "copying files"
I am developing a project for an STM32H563xxx HW and I have updated all the necessary libraries such as:
- ThreadX v6.2.0 (I cannot upgrade it to the 6.4...)
- FW package manager: STM32Cube FW_H5 V1.3.0
- And i am running the software on a WIndows 10 laptop
How is that? What can I do to solve this problem.