Skip to main content
Associate
March 4, 2024
Solved

Conversion DFU-File to Hex-File

  • March 4, 2024
  • 3 replies
  • 5173 views

I try to convert a DFU-File to a Hex-File with the ST-Tool  "DfuFileMgr.exe" from the DfuSe_v3.0.6 Toolkit.
The reason for the conversion is, that we have an Update-Application in the field that works with USP-DFU update and the old DfuSe driver. Now we would like to change to a new Application with the CubeProgrammer-API. With the CubeProgrammer-API we can download a HEX-File over DFU-USB. For compatibility reason we would like to use the old DFU-Files, convert it to HEX and upload it over DFU-USB with the CubeProgrammer-API. 

I tested the convrersion it with a "round-trip":
1. Start with a given hex-File: test.hex (see attachment)
2. Convert hex-to-dfu with DfuFileMgr.exe => test.dfu (see attachment)
3. Convert back dfu-to-hex with DfuFileMgr.exe => test_00.hex (see attachment)

The generated hex-File test_00.hex has now data on Address 0x0800_0000. The original hex-File test.hex starts on Address 0x0800_C000!!! The converted Hex-File is unusable.

I verified the original and the generated hex file. The wrong code block in the gererated file from address 0x0800_0000 - 0x0800_01E0 (placed on line 516-530 in file test_00.hex) can be found in the original hex from address 0x0801_0000 - 0x0801_01E0 (placed on line 1027-1056 in the file test.hex).
The same is for each section changes 0x0801, 0x0802 and 0x0803. Always a block from 480 bytes from address 0x0000-0x01E0.

Somehow the DfuFileMgr seems to have a problem with the first code block from the original hex file from address 0x0800_C000 - 0x0800_C1D8. The next row starts on 0x0800_C1E0. The addresses from 0x0800_C1D9 - 0x0800_C1E0 are not defined in the original hex-file.
Exact the first code blocks from 480 Bytes are missplaced on the entries of the sections 0x0800, 0x0801, 0x0802.

My questions:

1. Can the DfuFileMgr.exe handle undifined code blocks in a HEX-file?

2. Is it "only" a problem for the convertion from dfu to hex or is the dfu file itselfe also wrong for hex files ith undefined code blocks?
 

This topic has been closed for replies.
Best answer by urban17

Many thanks for the fast reply. Good to know there is a bug for hex files with undifined adress blocks.

I also tried now the other converters. The conversion to "S19" and "multiple bin" are working without error with the same input dfu.

As a workaround, we take two steps. First we extract a s19 file from the dfu with the DfuFileMgr and then we generate a hex file from it with the tool SRecord.

3 replies

Tesla DeLorean
Guru
March 4, 2024

The tool generating the .HEX from the .DFU is broken. The segment line comes too late as the content wraps between 0x0800FFE0 into 0x08010000. I could build a tool that does this properly

...

:20FFC000074997F907305B09012000FA02F241F8232000BF0C37BD465DF8047B704700BFCC
:20FFE00000E100E080B483B000AF03463960FB7197F90730002B0ADB3B68DAB20C4997F9F1
:2000000007301201D2B20B4483F800230AE03B68DAB20849FB7903F00F03043B1201D2B26C
:200020000B441A7600BF0C37BD465DF8047B704700E100E000ED00E080B489B000AFF8604F
:20004000B9607A60FB6803F00703FB61FB69C3F10703042B28BF0423BB61FB690433062BAA
:2000600002D9FB69033B00E000237B614FF0FF32BB6902FA03F3DA43BB681A407B699A4046
:200080004FF0FF317B6901FA03F3D9437B680B40134318462437BD465DF8047B704780B500
:2000A00082B000AF78607868FFF74CFF00BF0837BD4680BD80B586B000AF0346B9607A60D2
:2000C000FB7300237B61FFF761FF78617A68B9687869FFF7B1FF024697F90F30114618462E
:2000E000FFF780FF00BF1837BD4680BD80B582B000AF0346FB7197F907301846FFF754FF04
:2001000000BF0837BD4680BD80B584B000AF78607B689B6DFB60FEF785FCB8607B6893F86F
:200120003530DBB2022B08D07B6880225A657B68002283F83420012352E07B681B681A6872
:200140007B681B6822F016021A607B681B685A697B681B6822F080025A617B681B6C002B22
:2001600003D17B689B6C002B07D07B681B681A687B681B6822F008021A607B681B681A68F3
:200180007B681B6822F001021A6013E0FEF74AFC0246BB68D31A052B0CD97B6820225A65EB
:2001A0007B68032283F835207B68002283F83420032315E07B681B681B6803F00103002B6D
:2001C000E4D17B68DB6D3F229A40FB689A607B68012283F835207B68002283F834200023DA
:020000040801F1
:2001E00018461037BD4680BD80B483B000AF78607B6893F83530DBB2022B04D07B68802246
:200200005A6501230CE07B68052283F835207B681B681A687B681B6822F001021A60002335

...

test.dfu
0003034D

CRC32:6825DCD4 (Computed)

CRC32:00000000 (Computed Whole File)

0000 : 44 66 75 53 65 01 3D 03-03 00 01 DfuSe.=....

0003033D 1
0000 : 54 61 72 67 65 74 00 01-00 00 00 53 54 2E 2E 2E Target.....ST...
0010 : 00 3A 5C 00 65 6D 70 5C-68 65 78 5C 74 65 73 74 .:\.emp\hex\test
0020 : 2E 64 66 75 00 00 00 00-00 00 00 00 00 00 00 00 .dfu............
0030 : 00 00 00 00 00 00 00 00-00 00 00 00 00 00 00 00 ................
0040 : 00 00 00 00 00 00 00 00-00 00 00 00 00 00 00 00 ................
0050 : 00 00 00 00 00 00 00 00-00 00 00 00 00 00 00 00 ................
0060 : 00 00 00 00 00 00 00 00-00 00 00 00 00 00 00 00 ................
0070 : 00 00 00 00 00 00 00 00-00 00 00 00 00 00 00 00 ................
0080 : 00 00 00 00 00 00 00 00-00 00 00 00 00 00 00 00 ................
0090 : 00 00 00 00 00 00 00 00-00 00 00 00 00 00 00 00 ................
00A0 : 00 00 00 00 00 00 00 00-00 00 00 00 00 00 00 00 ................
00B0 : 00 00 00 00 00 00 00 00-00 00 00 00 00 00 00 00 ................
00C0 : 00 00 00 00 00 00 00 00-00 00 00 00 00 00 00 00 ................
00D0 : 00 00 00 00 00 00 00 00-00 00 00 00 00 00 00 00 ................
00E0 : 00 00 00 00 00 00 00 00-00 00 00 00 00 00 00 00 ................
00F0 : 00 00 00 00 00 00 00 00-00 00 00 00 00 00 00 00 ................
0100 : 00 00 00 00 00 00 00 00-00 00 20 02 03 00 02 00 .......... .....
0110 : 00 00 ..

00030220
0000 : 00 C0 00 08 D8 01 00 00- ........

0800C000 000001D8 (Basis / Length)

0000 : E0 C1 00 08 38 00 03 00- ....8...

0800C1E0 00030038

--------
00030220

0000 : 00 00 00 00 83 04 1A 01-55 46 44 10 D4 DC 25 68 ........UFD...%h

CRC32:6825DCD4 (Header)

.  

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
March 4, 2024

@Christian N please open a ticket on the DfuFileMgr tool failure, or indicate if further work / maintenance is going to be be done on such tools.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
urban17AuthorBest answer
Associate
March 7, 2024

Many thanks for the fast reply. Good to know there is a bug for hex files with undifined adress blocks.

I also tried now the other converters. The conversion to "S19" and "multiple bin" are working without error with the same input dfu.

As a workaround, we take two steps. First we extract a s19 file from the dfu with the DfuFileMgr and then we generate a hex file from it with the tool SRecord.