2013-09-10 7:45 AM
Hi,
For the moment I am using the channel2 of the Timer 2 in capture mode. At each rising edge of the signal, the timer is captured and reseted; It works fine; My code is this following:
GPIO_InitTypeDef GPIO_InitStructure;
/* GPIOC Periph clock enable */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);
/* Configure PB10 in input*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3 ;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;
GPIO_Init(GPIOB, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource3, GPIO_AF_TIM2);
/* Enable the TIM2 global Interrupt */
//configure NVIC
//select NVIC channel to configure
NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn;
//set priority to highest
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0;
//set sub-priority to highest
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x0;
//enable IRQ channel
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
//update NVIC registers
NVIC_Init(&NVIC_InitStructure);
// Timerx Periph clock enable
RCC_APB1PeriphClockCmd( SYNCH_TIMER_CLK, ENABLE );
// Configures the Timerx internal Clock
TIM_InternalClockConfig ( SYNCH_TIMER_BASE );
TIM_DeInit( SYNCH_TIMER_BASE );
TIM_TimeBaseStructInit( &TIM_TimeBaseStructure );
TIM_TimeBaseStructure.TIM_Prescaler = TIM_ICPSC_DIV1;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseStructure.TIM_Period = 0xFFFF;
TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;
// Initializes the Timerx Time Base Unit peripheral
TIM_TimeBaseInit( SYNCH_TIMER_BASE, &TIM_TimeBaseStructure );
TIM_ICInitStructure.TIM_Channel = TIM_Channel_2;
TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising;
TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI;
TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1;
TIM_ICInitStructure.TIM_ICFilter = 0x0;
TIM_ICInit(SYNCH_TIMER_BASE, &TIM_ICInitStructure);
TIM_SelectSlaveMode(SYNCH_TIMER_BASE , TIM_SlaveMode_Reset);
//
// SYNCH_TIMER_BASE->SMCR |= 0x04; /* timer in reset mode */
// SYNCH_TIMER_BASE->SMCR |= 0x70;
// SYNCH_TIMER_BASE->SMCR |= 0x80;
// TIM_SelectMasterSlaveMode(SYNCH_TIMER_BASE , TIM_MasterSlaveMode_Enable);
//
/* TIM enable counter */
TIM_Cmd(SYNCH_TIMER_BASE, ENABLE);
/* DISABLE the CC2 Interrupt Request */
TIM_ITConfig(SYNCH_TIMER_BASE, TIM_IT_CC2, ENABLE);
Now I would like to use the channel 3 , so My configuration is this following:
GPIO_InitTypeDef GPIO_InitStructure;
/* GPIOC Periph clock enable */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);
/* Configure PB10 in input*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 ;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;
GPIO_Init(GPIOB, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource10, GPIO_AF_TIM2);
/* Enable the TIM2 global Interrupt */
//configure NVIC
//select NVIC channel to configure
NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn;
//set priority to highest
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0;
//set sub-priority to highest
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x0;
//enable IRQ channel
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
//update NVIC registers
NVIC_Init(&NVIC_InitStructure);
// Timerx Periph clock enable
RCC_APB1PeriphClockCmd( SYNCH_TIMER_CLK, ENABLE );
// Configures the Timerx internal Clock
TIM_InternalClockConfig ( SYNCH_TIMER_BASE );
TIM_DeInit( SYNCH_TIMER_BASE );
TIM_TimeBaseStructInit( &TIM_TimeBaseStructure );
TIM_TimeBaseStructure.TIM_Prescaler = TIM_ICPSC_DIV1;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseStructure.TIM_Period = 0xFFFF;
TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;
// Initializes the Timerx Time Base Unit peripheral
TIM_TimeBaseInit( SYNCH_TIMER_BASE, &TIM_TimeBaseStructure );
/*TIMx_CCR3 must be linked to the TI3 input*/
SYNCH_TIMER_BASE->CCMR2 |= 0x01;
/* CC3S = 01 :: IC3 is mapped on TI3 */
TIM_ICInitStructure.TIM_Channel = TIM_Channel_3;
TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising;
TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI;
TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1;
TIM_ICInitStructure.TIM_ICFilter = 0x0;
TIM_ICInit(SYNCH_TIMER_BASE, &TIM_ICInitStructure);
TIM_SelectSlaveMode(SYNCH_TIMER_BASE , TIM_SlaveMode_Reset);
/* TIM enable counter */
TIM_Cmd(SYNCH_TIMER_BASE, ENABLE);
/* DISABLE the CC3 Interrupt Request */
TIM_ITConfig(SYNCH_TIMER_BASE, TIM_IT_CC3, ENABLE);
but with the channel 3, the reset mode doesn't work.
I don't understand why. Is it possible to do the same thing with channels 1/2 and channels 3/4 ?
Thank you very much,
GF.
#timer2-channel
2013-09-10 8:27 AM
You can't trigger a TIM from TI3 or TI4. You can push CH3 via the XOR to TI1
If you take CCRx measurements, captured via DMA for fast frequencies, you can compute a delta rather than reset. Note to All : When posting code try to post something that is sufficiently complete and free-standing that it compiles, and I don't have to guess/search what STM32 part you're using, or what the defines are.2013-09-11 2:16 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.