Code for STM32F779I Eval board
Hi STM Community, I am currently working on STM32F779I eval board for developing CAN, FreeRTOS with FatFs and SD card drivers.I have generated code using cube mx and imported into system workbench for STM32 IDE.
I tried to test the code for writing into SD card , But it is failing at fmount .
Then I tried Example code(Fatfs_uSD_RTOS) available for F769I eval board ,I build and flashed to F779I board, It is able to write to SD card successfully.
So I have doubt that what is the difference between these two eval boards, if no much differences are available can i use these code for f779i board for my further development. If not what are the changes I have to make f769i code.
As mentioned in one of the post
https://community.st.com/message/175333-building-samples-of-stm32cubef7
. I found only encryption support is difference .Please suggest me Whether to proceed with f769i code for f779i or else do I need to work on the generated code for f779i cube mx.
Thanks
#stm32f7