Skip to main content
sangamesh
Associate II
August 26, 2015
Question

Changing clock source from HSE to HSI

  • August 26, 2015
  • 5 replies
  • 1973 views
Posted on August 26, 2015 at 08:16

Hi 

Please refer below code to change clock source from external HSE to internal HSI

/* Enable HSE Oscillator and activate PLL with HSE as source */

#if 0 // Choose External Crystal (HSE) As Source

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;

RCC_OscInitStruct.HSEState = RCC_HSE_ON;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

RCC_OscInitStruct.PLL.PLLM = 25;

RCC_OscInitStruct.PLL.PLLN = 240;

RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;

RCC_OscInitStruct.PLL.PLLQ = 5;

HAL_RCC_OscConfig(&RCC_OscInitStruct);

#else // Choose Internal Crystal - 16MHz (HSI) As Source

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

RCC_OscInitStruct.HSEState = RCC_HSE_OFF;

RCC_OscInitStruct.HSIState = RCC_HSI_ON;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

RCC_OscInitStruct.PLL.PLLM = 16;

RCC_OscInitStruct.PLL.PLLN = 240;

RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;

RCC_OscInitStruct.PLL.PLLQ = 5;

HAL_RCC_OscConfig(&RCC_OscInitStruct);

#endif

/* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2

clocks dividers */

RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);

RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;

RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3);

We observed that the most of the peripherals are working fine with this change from HSE to HSI

however the USB host communication (PB14 PB15) which is connected to external HUB IC(which uses 48Mhz crystal) to communicate with 4 USB devices is not as same as we observed with HSE configuration.

Are we missing anything in changing from HSE to HSI, do we need to change anything somewhere else for USB host communication to work normal

Assist us on this
    This topic has been closed for replies.

    5 replies

    Nesrine M_O
    Associate
    August 26, 2015
    Posted on August 26, 2015 at 11:04

    Hi vandal.sangamesh,

    If I guess that you use one STM32F4xx product so according to any STM32F4 datasheet, The USB OTG full-speed controller requires a dedicated 48 MHz clock that is generated by a PLL connected to the HSE oscillator, then it means that it's unable to use HSI.

    For more information please refer to sections related to USB in your STM32 reference manual and datasheet.

    -Syrine-

    sangamesh
    sangameshAuthor
    Associate II
    August 26, 2015
    Posted on August 26, 2015 at 11:54

    Can we not generate the 48 MHz clock from PLL clocked by HSI oscillator (which we are already doing)?

     

    Nesrine M_O
    Associate
    August 26, 2015
    Posted on August 26, 2015 at 12:30

    According to the reference manual:

    “A main PLL (PLL) clocked by the HSE or HSI oscillator and featuring two different output clocks:

    – The first output is used to generate the high speed system clock (up to 180 MHz)

    – The second output is used to generate the clock for the USB OTG FS (48 MHz), the random analog generator (≤48 MHz) and the SDIO (≤48 MHz).�?

    In the case of USB OTG FS, the specification requires the use of HSE.

    -Syrine-

    John F.
    Associate III
    August 26, 2015
    Posted on August 26, 2015 at 12:47

    The USB clock must be accurate. HSI is not good enough so the external crystal oscillator must be used.

    Jith cr
    Associate II
    April 28, 2017
    Posted on April 28, 2017 at 08:24

    Hi ,

    Is it possible to use HSI for DCMI and LTDC ?