CDC_Transmit_FS is not happening from inside the CDC_Receive_FS function
Hi there,
I am trying to Transmit data over USB CDC after receiving a command, So I need call cdc transmit function inside cdc rx function in which I am comparing the received data.
But i am able to use only 1 cdc_tx function. when I am calling more than 1 tx function it is not functioning..
Following are the cdc tx and rx functions that I am using:-
uint8_t CDC_Transmit_FS(uint8_t* Buf, uint16_t Len)
{ uint8_t result = USBD_OK; /* USER CODE BEGIN 7 */ USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef*)hUsbDeviceFS.pClassData; if(USB_CONNECTED) { while(hcdc->TxState != 0); } /*if (hcdc->TxState != 0){ return USBD_BUSY; }*/ USBD_CDC_SetTxBuffer(&hUsbDeviceFS, Buf, Len); result = USBD_CDC_TransmitPacket(&hUsbDeviceFS);/* USER CODE END 7 */
return result;}static int8_t CDC_Receive_FS (uint8_t* Buf, uint32_t *Len)
{ /* USER CODE BEGIN 6 */ USBD_CDC_SetRxBuffer(&hUsbDeviceFS, &Buf[0]); //printf('\n\r%d\n\r',*Buf); if(Buf[0]=='i') { CDC_Transmit_FS((uint8_t *)'\n\r Hello\n\r',strlen((const char *)'\n\r
Hello
\n\r'
));CDC_Transmit_FS((uint8_t *)'\n\r
Hello\n\r',strlen((const char *)'\n\r
Hello
\n\r'
)); }USBD_CDC_ReceivePacket(&hUsbDeviceFS);
return (USBD_OK); /* USER CODE END 6 */ }I am using STM32F2 nucleo board
CubeMX v 4.22.0