cancel
Showing results for 
Search instead for 
Did you mean: 

Cant read/write from external sdram stm32f429, AS4C8M16S-6TIN

julius
Associate II
Posted on October 19, 2016 at 09:08

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
waclawek.jan
Super User
Posted on October 19, 2016 at 11:12

A0 and A1 stuck/not connected? Check activity with an oscilloscipe directly on the SDRAM's A0/A1 pins.

JW
julius
Associate II
Posted on October 19, 2016 at 12:24

Hi JW,

good gues, O thought it too. But then blocks of memory would be unredable, because address line is used to send colum and row adress so blocks of memory (4x4 cels) would be the same. Now only repetition 1x4 is the same. To be sure now I ***** signals with oscilloscope. You can see in attach I add A0 compare A1 address line and A1 compare A3 address line. As you can see, everything is fine. Also you can find attach 3, where i higlight adress lines from 0 to

Today I did one more reseach.

I noticed that if i continously write/read in SDRAM, sometimes I get values diferent than repeation of 4.

So write my array

write[100]and after that I read that array

read[100]. After read/write i compare these two array and if they not match, I stop writing, and left only reading part.

Rezult - I always get array with broken repeation 1x4. To be more clear:

Continously rea/write

__________________________________________

Write to sdram Read from sdram (most common)

0 300

100 300

200 300

300 300

400 700

500 700

600 700

700 700

800 1100

900 1100

1000 1100

1100 1100

1200 1500

1300 1500

1400 1500

1500 1500

After I capture one mismatch with comon read values i turn of writing

mismatch After turn of write (only continuous read left)

300 300

300 300

300 300

300 300

700 700

600 600

600 600

700 700

1100 1100

1100 1100

1000 1100

1100 1100

1500 1500

1500 1500

1500 1500

1500 1500

So the problem apears only on write sequence.

Thanks for answer anyway.

________________

Attachments :

A0_A1.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1KT&d=%2Fa%2F0X0000000blO%2FQ80Fhw8iuywyaFK3MjadTE.Wsqr4GVMQIsLxPf2JgKQ&asPdf=false

A1_A3.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1DZ&d=%2Fa%2F0X0000000blM%2Fsfs_SrLpjGu1bFNIFoDheRhTbbQAlcWCsB0KMKpuuzk&asPdf=false

Hardware.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1KJ&d=%2Fa%2F0X0000000blK%2F9qkPM02.O2IH5sbU5tCGjJ1.YLXRIT98iEFKb_h8qrs&asPdf=false
Posted on October 19, 2016 at 13:49

Your SDRAM lacks of sufficient power supply. 100nF capacitors to every VDD and VDDQ pin is necessary, HF Separation of VDD and VDDQ is strongly recommended. To make it even worse in your design, the SDRAM is sharing its 100nF Capacitory with the uC. See the Datasheet of the SDRAM, it draws 200mA during refresh cycle / 120mA in normal use. See attached file to see more Details ...

________________

Attachments :

SDRAM_Power.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1Fk&d=%2Fa%2F0X0000000blL%2FK1.MxLwTXYbtaa7tqZb4sHWZG9Mr4TrI6oZDHnehO_U&asPdf=false
Posted on October 19, 2016 at 14:04

See also attached schematics of STM32F4/7 Disco SDRAM with extra 100nF Capacitors for every VDD/VDDQ pin.

________________

Attachments :

SDRAM_DISCO.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1K0&d=%2Fa%2F0X0000000blJ%2F3Y105pHYLKetgaSEHsmZlaoVyfu5HTDRlmKEX2ASEg0&asPdf=false
julius
Associate II
Posted on October 20, 2016 at 10:50

Hello Markus, thank you for answer,

I try to connect 100 nF capacitors on each VDD and VDDQ pin (see in attatch). There is no shorts i tested all posible shorts with multimeter. But the result is the same.

Any more ideas, why this bug is appearing?

________________

Attachments :

soldered_100n_and_4.7uF_cap.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1K9&d=%2Fa%2F0X0000000blH%2FbsZARaawUCwg26AnVwFTKncHsbzwHHy6gpZzQhxoqV4&asPdf=false
waclawek.jan
Super User
Posted on October 20, 2016 at 11:17

I'd start with small steps: clear the entire memory (write 0), check it is clear, then write some nonzero value to a single address once, check entire memory for changes. Try with different values and different addresses, but always one write only. Come back with results.

JW
julius
Associate II
Posted on October 20, 2016 at 12:02

Hi JW,

Write zeroes to SDRAM was alredy done by initialization code. Folowing your instructions I implement test code:

 

 write[0]=0xFAFA;

 

 HAL_SDRAM_Write_16b(&g_sdram, 0xD0000000+111112, &write, 1);  // values I tried: 0, 12, 112, 1112, 11112 and 111112

 

 for (i=0; i<0x400000; i+=2)   // 0x400000 - ram size, based on uint16_t words

 

 {

 

  HAL_SDRAM_Read_16b(&g_sdram, 0xD0000000+i, &read, 1);

 

   if (read[0]==0)

 

 read[0]=0;

 

   else if (read[0]!=0xFAFA)

 

 read[0]=read[0];              // breakpoint 1

 

   else if (read[0]==0xFAFA)

 

 read[0]=read[0];             // breakpoint 2

 

 }

 

Rezult: I always 4 times stoped on breakpoint 2, which indicates writed value in 4 cells after 1 write cycle, and then I get end of the for cycle. Breakpoint 1 newer occured. I do not put breakpoint on first if, because most of memory is zero.

Note: I have more than one sample, all act the same

Any ideas?
waclawek.jan
Super User
Posted on October 20, 2016 at 12:48

I've just noticed:

 

>  sdramCommand.ModeRegisterDefinition =(uint32_t)  SDRAM_MODEREG_BURST_LENGTH_2             |       

 

 

I believe FMC does not support bursts on the SDRAM-interface. RM0090 rev.13 in 37.7.3  SDRAM controller functional description, SDRAM initialization checklist, item 7:

 

The Burst Length (BL) of 1 must be selected by configuring the M[2:0] bits to 000

 

in the mode register (refer to the SDRAM datasheet).

Please review. I am no FMC/SDRAM expert.

JW

julius
Associate II
Posted on October 20, 2016 at 13:08

Acording to your note, I changed this part to:

 

  sdramCommand.ModeRegisterDefinition =(uint32_t)  SDRAM_MODEREG_BURST_LENGTH_1             | // ((uint16_t)0x0000)

 

                                          SDRAM_MODEREG_BURST_TYPE_SEQUENTIAL      | // ((uint16_t)0x0000)

 

                                                         FMC_SDRAM_CAS_LATENCY_3                  | // ((uint16_t)0x0030)

 

                                                       SDRAM_MODEREG_OPERATING_MODE_STANDARD    | // ((uint16_t)0x0000)

 

                                                         SDRAM_MODEREG_WRITEBURST_MODE_SINGLE;      // ((uint16_t)0x0200)

 

Unfortunately i get the same rezult. I have also tried to change this row:

  g_sdram.Init.ReadBurst = FMC_SDRAM_RBURST_ENABLE;

 

But nothing happened.

Any more ideas?