Cannot connect to Board anymore
Hi,
i designed a board with a STM32F030 and already flashed and debugged it with success. However i used a Nucleo Board in order to flash it and I cannot connect to the target anymore. I also want to mention that i used the regular ST-LINK V2 as well. I already tried to power the target, while bridging BOOT0 to +3V3 and I also tried to erase the memory with ST-Util. In fact nothing works (OpenOCD, ST-UTIL, texane st-util Command Line Tool...). I already checked some threads with similar problems, however I couldn't find a solution so far. Has anyone else had a problem like this?