Skip to main content
Matt Roybal
Associate III
January 29, 2018
Solved

Can you change SWO output to a different GPIO? I want to use the SPI that conflicts with the SWO, but still need to printf on SWO.

  • January 29, 2018
  • 5 replies
  • 1285 views
Posted on January 29, 2018 at 21:09

Hello, I am using STM32F103 and STM32F301. I need to use the SPI that shares the same pin as SWO. Is it possible to move the SWO to a different pin so I can retain the printf to console functionality for debugging?

    This topic has been closed for replies.
    Best answer by Tesla DeLorean
    Posted on January 29, 2018 at 21:29

    Only PB3 supported. Use a USART_TX as an alternative. 

    5 replies

    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    January 29, 2018
    Posted on January 29, 2018 at 21:29

    Only PB3 supported. Use a USART_TX as an alternative. 

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Matt Roybal
    Associate III
    January 29, 2018
    Posted on January 29, 2018 at 22:29

    Hi Clive, thanks for the info! So I just need to chose a group of pins, such as RX1/TX1, TX2/TX2, RX3/TX3 and get a UART protocol running on those pairs?

    Andrew Neil
    Super User
    January 30, 2018
    Posted on January 30, 2018 at 10:47

    SWO =

    S

    erial

    W

    ire

    O

    utput - as the name suggests, it is output (Tx) only.

    http://infocenter.arm.com/help/topic/com.arm.doc.ddi0314h/Chdhgebe.html

     

    So there would be no need to reserve an Rx pin for equivalent funcitonality

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    T J
    Senior III
    January 29, 2018
    Posted on January 29, 2018 at 23:58

    In the cube, you can hold <cntl> and click the pin to see alternatives, for the SPI port, I mean...

    T J
    Senior III
    January 30, 2018
    Posted on January 30, 2018 at 07:10

    You use the cube software, to see the available pins for your requirements.

    Did you use the cube before ?

    Edit:

    before the cube there is the reference material;

    PM0214   STM32F3 and STM32F4 Series Cortex®-M4 programming manual.

    Also, in the processor data sheet

    look for PA9  in the alternate function pin map.

    here you can see all the variations of all the pins.