Question
Can the ADC regular channel and injected channel of STM32G4 not be used at the same time? Is this a bug?
I use cubemx (6.0.0) to generate ADC1 configuration code, for example, ADC1 channels 1, 2, and 3 are injection channels, and TIM1 channel 4 is used to trigger, and ADC1’s 4, 5 are Regular channel. STM32F4 can work very well. But STM32G4 does not work, the regular channel does not run.