Can I use HSE oscillator clock for bxCAN?
Hi,
Currently, I'm working on a project where LCD, Camera and CAN are involved.
I'm using STM32F769I-EVAL platform for my work with 'SetupSTM32CubeMX-4.19.0' installation and 'STM32Cube_FW_F7_V1.6.0' firmware package.
As far as my understanding, Camera and LCD required accurate clocks hence, I have to use HSE oscillator clock for the same.When it comes to bxCAN, I have seen many of the example source initialize HSI clock for the same. When I try to make it into HSE, then BxCAN is not functioning properly!
The only CAN example I have found with HSE clock is 'CAN_Networking' example from
'
STM32Cube_FW_F7_V1.6.0' firmware package, in which only one side (transmitting) is working properly and other side (receiving) not.
So, I would like to know whether bxCAN can work with HSE oscillator clock. If yes, then which values (such as SYSCLK,HCLK, AHB Prescaler, PLLM etc. ) I have to put for the HSE clock configuration in-order to make it work for LCD, Camera and CAN.
Thank you in advance,
Ajith P V#hse-config #stm32f769i-eval #can-bxcan #clock-configuration #stm32f7 #hsi #stm #stm32