Question
Can I use higher speed than 400kHz with I2C with STM32F439
Posted on October 14, 2017 at 21:43
Dear ,
Currently I use a STM32F439. I have a demand to increase the speed of I2C above 400kHz. Is this possible? If not is there a STM32F/L4 controller that is pin-2-pin compatible that can be used instead?
Regards,
Roland
#i2c-fast-mode-+-stm32f439