Skip to main content
Associate
January 10, 2025
Solved

Bug in stm32h7xx_hal_spi.c when using HAL_SPI_TransmitReceive_IT()

  • January 10, 2025
  • 3 replies
  • 937 views

I believe I discovered a bug in the SPI driver in relation to using HAL_SPI_TransmitReceive_IT() that causes buffer overflows, which also made it tricky to discover.

In our project, I had switched our SPI handlers to from blocking to non-blocking using the interrupt APIs.

The bug happens when calling HAL_SPI_TransmitReceive_IT() which hits:

HAL_StatusTypeDef HAL_SPI_TransmitReceive_IT(SPI_HandleTypeDef *hspi, const uint8_t *pTxData, uint8_t *pRxData, uint16_t Size)
{
 ...
 /* Fill in the TxFIFO */
 while ((__HAL_SPI_GET_FLAG(hspi, SPI_FLAG_TXP)) && (tmp_TxXferCount != 0UL))
 {
 ...
 hspi->pTxBuffPtr += sizeof(~);
 hspi->TxXferCount--; // <--- This decrements until 0
 ...

 Then when an interrupt hits for SPI_TxISR_32BIT, SPI_TxISR_16BIT, or SPI_TxISR_8BIT it hits:

static void SPI_TxISR_8BIT(SPI_HandleTypeDef *hspi)
{
 /* Transmit data in 8 Bit mode */
 *(__IO uint8_t *)&hspi->Instance->TXDR = *((const uint8_t *)hspi->pTxBuffPtr);
 hspi->pTxBuffPtr += sizeof(uint8_t);
 hspi->TxXferCount--; // <---- Decrement without check, causing a rollover therefore an overflow

I fixed this locally by adding a condition check in the TxISR and RxISR handlers to this:

static void SPI_TxISR_8BIT(SPI_HandleTypeDef *hspi)
{
 /* Transmit data in 8 Bit mode */
 *(__IO uint8_t *)&hspi->Instance->TXDR = *((const uint8_t *)hspi->pTxBuffPtr);

 if(hspi->TxXferCount > 0) // <--- Make sure not zero
 {
 hspi->pTxBuffPtr += sizeof(uint8_t);
 hspi->TxXferCount--;
 }

Let me know your thoughts.

Regards.

Best answer by Saket_Om

Hello @AGreen 3rdEye 

The issue has been resolved, and the fix is now available on GitHub.

 

3 replies

ST Technical Moderator
January 10, 2025

Hello @AGreen 3rdEye ,

Thank you for having reported this issue.

An internal ticket number 200212 is submitted in order to review and check this.

(PS: Internal ticket number is only for reference, not available outside of ST)

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
January 17, 2025

Hi @AGreen 3rdEye 

Issue is confirmed and our team is working to resolve this for impacted SPI HAL.

Thank you for your contribution.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Saket_OmBest answer
ST Technical Moderator
September 16, 2025

Hello @AGreen 3rdEye 

The issue has been resolved, and the fix is now available on GitHub.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om