Skip to main content
dieter 123
Associate III
April 4, 2017
Question

automotive certified STM32?

  • April 4, 2017
  • 10 replies
  • 7614 views
Posted on April 04, 2017 at 16:28

Hi

I am supposed to develop a 'simple' automotive project drive some interior car lights controlled by CAN.

Which ST controller is best suited for this? (Cheapest and smallest)

Are any of the STM32 certified for automotive ?

Is there a ST controller with built in CAN interface?

Does ST have a certified CAN protocol stack?

If not which one would you recommend?

Thx

    This topic has been closed for replies.

    10 replies

    Tesla DeLorean
    Guru
    April 4, 2017
    Posted on April 04, 2017 at 16:43

    Would also be interested in a +125C rated part, even at reduced spec, a lot of applications/locations where +85C won't suffice.

    What is the constraining factor here? FLASH? Programming/retention?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    waclawek.jan
    Super User
    April 4, 2017
    Posted on April 04, 2017 at 17:10

    +125C

    There are a few mentioned, look for

    3 = Industrial temperature range, - 40 to 125 °C

    suffix. I don't know how hard it may be to chase them down in the wild.

    JW

    0690X00000606h5QAA.png
    Tesla DeLorean
    Guru
    April 4, 2017
    Posted on April 04, 2017 at 17:17

    Ok, mostly seen 6 (Commercial) and 7 (Industrial) suffix devices

    ST might want to pull this into their IoT focus, while Car/Automotive might be the primary internal driver, the use of stuff above 85C gets to be important deploying IoT devices into inhospitable environments, where direct sunlight and ambient temperature are high, and cooling is not available/practical.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Max
    ST Employee
    April 5, 2017
    Posted on April 05, 2017 at 05:24

    Hello,

    There is no STM32 with automotive qualification. Automotive qualification is much more than just the temperature...

    There are 125C temperature version in the following families:

    - STM32F4 access line (STM32F401, STM32F410, STM32F411, STM32F413, STM32F423)

    - most STM32L0

    - most STM32L4 

    complete list

    http://www.st.com/content/st_com/en/products/microcontrollers/stm32-32-bit-arm-cortex-mcus.html?querycriteria=productId=SC1169$$962=125|125

    STM8AL and STM8AF are qualified for automotive.

    There are 125C and even 150C versions available.

    STM8AF52xx have a CAN interface and certified driver can be purchased from vector software.

    Best regards,

    Max

    waclawek.jan
    Super User
    April 5, 2017
    Posted on April 05, 2017 at 10:33

    complete list

    /external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fst_com%2Fen%2Fproducts%2Fmicrocontrollers%2Fstm32-32-bit-arm-cortex-mcus.html%3Fquerycriteria%3DproductId%3DSC1169%24%24962%3D125%7C125

    I have used the same filter on that table. Sadly, it does not indicate real availability at the ''garage-scale'' distributors.

    And not only that:

    0690X00000606heQAA.png

    I understand why, it's just that it's again misleading and does not help in searching.

    I don't try the ''selector'', as I won't install Java (wonder why would that need to be so).

    JW

    Amel NASRI
    ST Technical Moderator
    May 22, 2017
    Posted on May 22, 2017 at 16:11

    Hi Jan,

    The selector is behaving in a way that it marks a line as active as soon as at least one given device belonging to this line is active.

    This is the case for STM32F413RG.

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    alexborysevych9
    Associate II
    October 22, 2017
    Posted on October 22, 2017 at 19:58

    I'm working at big US automotive manufacturer.

    And the automotive STM32 is my biggest wish. Hopefully someday ST will do AEC-Q100 certified STM32F4 or similar chip. At the moment we are stuck with SPC and STM8, which are nice, but STM32 is the best!