Skip to main content
richard239955_stm1
Associate III
December 7, 2017
Question

Are these appropriate LoRaWAN learning tools

  • December 7, 2017
  • 14 replies
  • 2212 views
Posted on December 07, 2017 at 03:29

I own a NUCLEO-L053R8.

Is it appropriate to get a I-NUCLEO-LRWAN1, plug it into the NUCLEO  and use the I-CUBE-LRWAN (STM32CubeExpansion_LRWAN_V1.1.2) to start learning LoRaWAN?

Is the NUCLEO-L053R8 with the I-NUCLEO-LRWAN1 plugged in essentially the same as a B-L072Z-LRWAN1???

    This topic has been closed for replies.

    14 replies

    Andrew Neil
    Super User
    December 7, 2017
    Posted on December 07, 2017 at 16:21

    Why risk it?

    Why not just get a B-L072Z-LRWAN1 Discovery board, or a P-Nucleo-LRWAN1 kit?

    http://www.st.com/en/evaluation-tools/b-l072z-lrwan1.html

     

    http://www.st.com/en/evaluation-tools/p-nucleo-lrwan1.html

     

    That way, you know you have a complete kit, and you get ready-to-run examples specifically made for it - no messing about with trying to ensure that everything is compatible.

    Simples!

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    December 7, 2017
    Posted on December 07, 2017 at 16:28

    Is the NUCLEO-L053R8 with the I-NUCLEO-LRWAN1 plugged in essentially the same as a B-L072Z-LRWAN1???

    Ah - no, it isn't.

    The 

    I-NUCLEO-LRWAN1 has a USI module and is really just intended as a dumb modem - using AT commands:

    http://www.st.com/en/evaluation-tools/i-nucleo-lrwan1.html

     

    The USI module has a 

    Semtech SX127

    2

    radio.

    As noted elsewhere, the USI documentation is, well, 'lacking' ...

    >:(

    The Discovery board uses a muRata module with SX127

    6

    , and is well documented.

    Note that the 

    P-Nucleo-LRWAN1 kit also use the 

    SX127

    2

    .

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Tesla DeLorean
    Guru
    December 7, 2017
    Posted on December 07, 2017 at 16:33

    The USI part can be reprogrammed, but it's a non-ideal development platform. The LRWAN that ST supplies is relatively portable across boards and platforms.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Andrew Neil
    Super User
    December 7, 2017
    Posted on December 07, 2017 at 16:39

    Indeed - but the OP specifically asked about this as a starting point.

    Of course, stuff can be ported & adapted - but I really don't think that's great as

    a

    starting

    point.

    tomkins.richard

    ‌ -

    Turvey.Clive

    ‌ has postedextensively about his adventures with this stuff - including the porting across various boards...

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Tesla DeLorean
    Guru
    December 7, 2017
    Posted on December 07, 2017 at 16:52

    The P-NUCLEO-LRWAN1 package includes both shield and Nucleo board ($70), it is the most expensive path. You can buy the shield and board separately more cheaply. The SX1272 shield can be bought more cheaply $25, and a Nucleo for $10, but you already have that.

    https://www.mouser.com/ProductDetail/Semtech/SX1272MB2DAS/?qs=5aG0NVq1C4w5nso72Adcfw%3d%3d

     

    https://www.mouser.com/ProductDetail/STMicroelectronics/P-NUCLEO-LRWAN1/?qs=LtAzLad%252boeUT0TtoCWMp6w%3d%3d

     

    The B-L072Z-LRWAN1 is a different beast, and perhaps the optimum development/learning platform. The L0 has 192KB of FLASH, and the module uses the SX1276 radio.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    December 7, 2017
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..