Skip to main content
Jordi Becares
Associate III
July 2, 2018
Question

AN3966 over DevKit407 (STM32F407G-DISC1 + STM32F4DIS-BB) with TrueSTUDIO (Atollic)

  • July 2, 2018
  • 5 replies
  • 1261 views
Posted on July 02, 2018 at 18:17

Hi All, 

I have a DevKit407 (STM32F407G-DISC1 + STM32F4DIS-BB) and I'm working with AN3966.

I'm using the newest version of TrueSTUDIO

Exactly, I'm trying to run httpserver_socket (with FreeRTOS) over Board.

I know that there are a lot of threads about this topic, but I can not get to run it.

My problem is that app not compile. After import project from source code examples of AN3966 (stsw-stm32070), when I try to compile the IDE said some files are not found.. for example:

..\..\..\..\..\..\Utilities\Third_Party\lwip-1.4.1\src\core\ipv4\inet.c:41:23: fatal error: lwip/inet.h: No such file or directory

But the code is just imported from example...

I tried to modify the MCU the exact model, but I got the same error.

And, I tried to make a simply led blinking from STm32CubeMX and it works.

I think that it has to be a 'easy' step, simply run a example, so I think that maybe I'm skiping some step.

Please can you help me?

(Sorry if the solution is already posted, but I found for a lot of hours, and I didn't find the solution)

Thanks!

Jordi

#atollic-truestudio #devkit407 #lwip #an3966
This topic has been closed for replies.

5 replies

AvaTar
Senior III
July 3, 2018
Posted on July 03, 2018 at 07:27

The F407 Discovery itself has no Ethernet, so ST's Firmware package has no ..\Utilities\Third_Party\lwip-xxx sources.

There is a firmware package for the STM32F4DIS-BB board, downloadable somewhere on the Element14 webpage.

Pretty sure you can find it yourself.

Last time I tried the ethernet/webserver example from that package build 'out of the box'.

Jordi Becares
Associate III
July 3, 2018
Posted on July 03, 2018 at 08:19

Dear AvaTar,

thanks for your feedback.

But, I have full source code for lwip-xxx. I can see all files.

I downloaded the example from

https://www.st.com/en/embedded-software/stsw-stm32070.html

Furthemore, when I follow the error that shows the console I can open the file that compiler says 'not found'.

So, I think it's a problem of include path in example, but I don't understand. It's a ST official ApplicationNote, it has to be 'plug&play'.

Someone check AN3966 over F407Dis with TrueStudio (Version: 9.0.1 Build id: 20180420-1214). I'm work over Win10

Thanks

Jordi

AvaTar
Senior III
July 3, 2018
Posted on July 03, 2018 at 08:43

So, I think it's a problem of include path in example, but I don't understand. It's a ST official ApplicationNote, it has to be 'plug&play'.

Does it come with a project/workspace for Truestudio ?

I guess you expect a bit much here ... ;)

Adding an include path is a simple exercise. I use Crossworks, wich has no 'out of the box' support from ST. For porting aproject, I always spent the first 15 minutes assembling the source files, include paths and link libraries.