Skip to main content
liujun6037
Visitor II
November 9, 2014
Question

ALIENTEK Explorer STM32F407 Board Support AVI(mjpeg) player,resource share�

  • November 9, 2014
  • 1 reply
  • 1066 views
Posted on November 09, 2014 at 13:21

The Explorer STM32F407Development board is developed by ALIENTEK ,It is a very powerful, Here is the main features:

1,support AVIvideo play。up to 25fps for 320*240 and 10fps for 480*

2,support mp3/wav/flac/ape music play.up to 192K@24bit for wav.

3,support NES emulator,with apu&map,up to 480*480 solution.

4,support jpg/jpeg/gif/bmp picture view.

5,imitation IOS GUI。

Download the source code:

http://www.openedv.com/posts/list/139htm?fromAll=0

Here is the video:

http://v.youku.com/v_show/id_XODE2NDcwNzE2.html

Explorer STM32F407 pictures:

0690X00000605BmQAI.png0690X00000604OXQAY.png

The following pictures are from screenshot:

0690X00000605C6QAI.png0690X00000605BwQAI.png0690X00000605C1QAI.png0690X00000605CBQAY.png0690X000006056yQAA.png0690X00000605CGQAY.png0690X00000604UeQAI.png0690X00000605D9QAI.png See attachments

#stm32f407-explorer-alientek-avi

    This topic has been closed for replies.

    1 reply

    pkumar1883
    Associate III
    January 13, 2016
    Posted on January 13, 2016 at 07:17

    looks very cool kit. Is OS available in English?