cancel
Showing results for 
Search instead for 
Did you mean: 

After update to version 1.9 IDE, Bus I2C not working. Using IDE 1.8, I2C works fine.

RDos
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
TDK
Super User

Do a diff on the code between the two and see what's different.

If you feel a post has answered your question, please click "Accept as Solution".
RDos
Associate II

There is no difference, it's the same code.

File ioc was migrated from 6.4 to 6.5

IDE 1.8

HAL 1.16.2

Toolchain 9-2020-q2

IDE 1.9

HAL 1.16.2

Toolchain 10.3-2021.10

If the code is actually the same, has to be the compiler causing changes. Unlikely to be an issue with the GCC compiler, more likely to be a software bug being exposed by slightly different compilations.
Regardless, going to be hard to diagnose without details.
If you feel a post has answered your question, please click "Accept as Solution".

V. 1.9 uses a newer toolchain by default (compiler GCC 10).

RDos
Associate II

using ide 1.9 and Toolchain 9-2020-q2

works well.