ADC1 behaving strangely on a STM32L496AGI6.
- June 19, 2020
- 5 replies
- 1759 views
Hi forum.
I have a question regarding the STM32L496G-discovery board. I want ADC1 to sample PC4 located on the on board Arduino connector, take 10 samples for this example and have the DMA xfer these to memory.
I have a CubeIde project set up and have set up all the ADC and DMA components to work. This same project works as expected when I use the NUCLEO-L496ZG which is fitted with the STM32L496ZGT6U, but when I run the same code on the STM32L496G-discovery board which is fitted with a STM32L496AGI6, I find the output from the ADC sits about mid point.
Then when I take the analog pin PC4 to ground or 3V, nothing happens.
I have looked into the ref manual, and in fact this was the same data I used when setting this example up for the NUCLEO-L496ZG, but I cannot find anything that may be specific to the STM32L496AGI6.
Has anyone had the same experience. Is there something strange about the
STM32L496G-discovery board, or is the problem with my understanding. I have posted my setup code, I hope that helps clear up what I talking about.
By the way the only ADC sampling I can see in the STM32L496G-discovery boards schematic is for the IDD measure which feeds in to on board MFX_V3, a STM32L152CCT6, so there seems to be no other ADC use.
Thanks.