cancel
Showing results for 
Search instead for 
Did you mean: 

ADC EOC Interrupt

blimmer
Associate II
Posted on May 30, 2011 at 15:08

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
blimmer
Associate II
Posted on May 30, 2011 at 16:41

P.S.:

The part

void ADC1_2_IRQHandler(void)

{...}

is the only part where I cannot set any breakpoints in my compiler. Though I don't know if thats significant concerning my problem...

Anybody got a hint for me?

Sincerely,

B.L.
raptorhal2
Lead
Posted on May 31, 2011 at 15:34

I don't know if this is your problem, but you are disabling ADC2 EOC despite the comment field.

Also, I would move the NVIC initialization function call to just after the RCC initialization function call.

Cheers, Hal

raptorhal2
Lead
Posted on June 01, 2011 at 01:18

For my IDE, I have to set the vector table base location at 0x8000000 as part of the NVIC initialization. If Ride 7 doesn't do that for you automagically, that might be the problem.

Cheers, Hal

blimmer
Associate II
Posted on June 02, 2011 at 15:37

Hello baird.hal.001,

thanks for your answers.

I've been able to solve the problem meanwhile.

Apparently the problem was the name of the used IRQ handler. I had used the ADC1_2_IRQHandler but instead I had to use ADC1_IRQHandler.

It's just a bit annoying that I spent about a week on solving this problem that I had just because the right handler can't be found neither in the manual nor in the toolchain I'm using.

In the newest documnetation only the (wrong) ADC1_2_IRQHandler can be found...

B.L.