Skip to main content
FB1
Associate II
Feb 18, 2023 8:35 PM UTC
Solved

USB Audio for STM32H723

I am looking for an example for USB audio device class UAC1 for NUCLEO-H723ZG.

The aim is to stream audio data from STM32 onto an android device (and there to a spectrum app). Many thanks to any hints.

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Feb 20, 2023 7:08 AM UTC

Hello @FB​ and welcome to the Community :)

You can follow the available application which is a part of the USB Device Library package within STM32CubeH7 firmware package:

\STM32Cube_FW_H7_Vx.x.x\Projects\STM32H743I-EVAL\Applications\USB_Device\Audio_Standalone

The example use USB device application based on the AUDIO Class implementation of an audio streaming on the STM32H7xx devices.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

1 reply

Imen.DBest answer
ST Technical Moderator
Feb 20, 2023 7:08 AM UTC

Hello @FB​ and welcome to the Community :)

You can follow the available application which is a part of the USB Device Library package within STM32CubeH7 firmware package:

\STM32Cube_FW_H7_Vx.x.x\Projects\STM32H743I-EVAL\Applications\USB_Device\Audio_Standalone

The example use USB device application based on the AUDIO Class implementation of an audio streaming on the STM32H7xx devices.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks