Skip to main content
PIvan.9
Associate III
September 2, 2021
Question

How to configure AcousticBF library for PCM mode on STM32L476RG?

  • September 2, 2021
  • 0 replies
  • 812 views

I'm trying to implement AcousticBF library functions and what I've noticed is that, when I configure it like this for PCM mode, 2 microphones:

void Audio_Libraries_Init(void)
{
 volatile uint32_t error_value = 0;
 /* Enable CRC peripheral to unlock the library */
 __CRC_CLK_ENABLE();
 /*Setup Beamforming static parameters*/
 error_value = 0;
 libBeamforming_Handler_Instance.algorithm_type_init=ACOUSTIC_BF_TYPE_CARDIOID_BASIC;
 libBeamforming_Handler_Instance.ref_mic_enable=ACOUSTIC_BF_REF_ENABLE;
 libBeamforming_Handler_Instance.ptr_out_channels=2;
 libBeamforming_Handler_Instance.data_format=ACOUSTIC_BF_DATA_FORMAT_PCM;
 libBeamforming_Handler_Instance.sampling_frequency=16;
 libBeamforming_Handler_Instance.ptr_M1_channels=1;
 libBeamforming_Handler_Instance.ptr_M2_channels=1;
 libBeamforming_Handler_Instance.delay_enable = 0;
 (void)AcousticBF_getMemorySize(&libBeamforming_Handler_Instance);
 libBeamforming_Handler_Instance.pInternalMemory =(uint32_t *)malloc(libBeamforming_Handler_Instance.internal_memory_size);
 error_value = AcousticBF_Init(&libBeamforming_Handler_Instance);
 
 /*Error Management*/
 if(error_value != 0U)
 {
 Error_Handler();
 }
 
 /*Malloc Failure*/
 if(libBeamforming_Handler_Instance.pInternalMemory == NULL)
 {
 Error_Handler();
 }
 
 /*Setup Beamforming dynamic parameters*/
 lib_Beamforming_Config_Instance.algorithm_type = ACOUSTIC_BF_TYPE_CARDIOID_BASIC;
 lib_Beamforming_Config_Instance.M2_gain = 0.0f;
 lib_Beamforming_Config_Instance.mic_distance = 212;
 lib_Beamforming_Config_Instance.volume = 24;
 error_value = AcousticBF_setConfig(&libBeamforming_Handler_Instance, &lib_Beamforming_Config_Instance);
 
 /*Error Management*/
 if(error_value != 0U)
 {
 Error_Handler();
 }
}

then, AcousticBF_FirstStep function returns 0, so I can't implement AcousticBF_SecondStep() function further:

void AudioProcess(void)
{
 if(AcousticBF_FirstStep(&((uint8_t *)(PCM_Buffer))[0],&((uint8_t *)(PCM_Buffer))[1], (int16_t *)Out_Buffer, &libBeamforming_Handler_Instance) == 1U)
 {
 SW_Task1_Start();
 }
 
 /*for L4 PDM to PCM conversion is performed in hardware by DFSDM peripheral*/
 Send_Audio_to_USB((int16_t *)Out_Buffer, (AUDIO_IN_SAMPLING_FREQUENCY/1000)*AUDIO_IN_CHANNELS);
}

Is there smth I missed? Or did I configure smth wrong?

This topic has been closed for replies.