Skip to main content
Associate III
April 29, 2025
Solved

Unable to write to RAW Structur in MC Motor Pilot

  • April 29, 2025
  • 1 reply
  • 291 views

Hello,

I am trying to write to SPEED_RAMP using the Registers tab in MC Control Pilot, however I get the following error:

ASPEP_RESP ERROR:ERROR_BAD_RAW_FORMAT

I am writing the data as follow for example: 6000;500

Can someone help me find the right synthax?

 

Thank you

This topic has been closed for replies.
Best answer by Fabrice LOUBEYRE

Hi AnthonyK, unfortunately this RAW format write feature into the Register Tab is not supported by the MCSDK Motor Pilot tool. You can only change SPEED_RAMP values from the Application/Speed Ramp boxes. 

Best Regards.

Fabrice

1 reply

Fabrice LOUBEYRE
Fabrice LOUBEYREBest answer
ST Employee
May 16, 2025

Hi AnthonyK, unfortunately this RAW format write feature into the Register Tab is not supported by the MCSDK Motor Pilot tool. You can only change SPEED_RAMP values from the Application/Speed Ramp boxes. 

Best Regards.

Fabrice