2022-04-20 11:48 PM
Are there any plans to make a Linux version of the Motor Control Workbench.
2022-04-25 2:02 AM
Hello @Sune Jensen,
Yes, the technology used in MCSDK6.0.0 is now cross-platform and Linux versions are in the pipe.
Regards
Cedric
2022-04-27 4:54 PM
How about a Mac version? Same story?
Mike
2023-12-13 2:25 AM
Seeing that all released versions of MCSDK6 still only supports windows, do you have any new information about the timeline for Linux support?
2024-08-20 1:08 AM - edited 2024-08-20 1:08 AM
Any updates on this? We are still only able to download the Windows-version.
2025-09-04 8:37 AM
Hi @cedric H
Its been a while since you said the Linux version is in the pipe. Is there any progress? Seems it must be quite a long pipe.. Realistically is this ever going to happen? It is very inconvenient having to support a seperate machine just to support the motor workbench, it really would be very helpful to be able to manage the whole project on Linux instead of only half.
Thanks.
Clive