Skip to main content
DTrif.1
Visitor II
February 24, 2020
Solved

Steval - spin3204 and motor jk86bls71-03-x001

  • February 24, 2020
  • 1 reply
  • 943 views

Hello. I am using Steval - spin3204 and motor jk86bls71-03-x001. I am building a project for Keil in ST Motor control 5.4.3. But I can’t start the engine with or without Hall sensors. I tried to make various configurations of PID controllers, PWM parameters, time, etc., but nothing works. Please tell me, if someone has a working project so that I can do it by analogy. A project that is located on the ST website is compiled with errors.

Here is the project I'm working with

This topic has been closed for replies.
Best answer by Claire O.

Hello DTrif.1,

Are you using the following example from the MCSDK5.4.3:

  • Six-Step drive with STSPIN3204

Thanks and best regards,

Claire

1 reply

Claire O.
Claire O.Best answer
ST Employee
April 3, 2020

Hello DTrif.1,

Are you using the following example from the MCSDK5.4.3:

  • Six-Step drive with STSPIN3204

Thanks and best regards,

Claire