Associate
June 22, 2025
Question
ST Motor Control Workbench Not Detecting STM32CubeMX
- June 22, 2025
- 4 replies
- 939 views
Hello everyone,
I am currently using ST Motor Control Workbench v6.4.0 along with STM32CubeMX v6.14.1 installed on my Windows PC. Although STM32CubeMX is correctly installed and working independently, when I click "Generate Code" in the Motor Control Workbench, the program fails to detect STM32CubeMX. It shows the message:
“STM32CubeMX not found – ver. '6.0.0' or higher is required.”
With that, I am not able to detect "Target Toolchain" and "Firmware Package Version" on Motor Control Workbench 6.4.0
I would be grateful if you could assist or provide confirmation regarding this workaround or a more official solution in case of future updates.