MC Workbench cannot generate projects with CubeMX 6.3.0
- July 22, 2021
- 1 reply
- 1396 views
Hi all,
I am using MC Workbench to generate motor projects.
As I upgrade my STM32CubeMX to 6.3.0, it doesn't work anymore.
I can directly use STM32CubeMX, but cannot generate source via MCWorkbench.
I tried MC Workbench 5.4.4, 5.4.6, 5.Y.1, and all of them failed to generate.
I noticed that when using CubeMX 6.3.0, it will popup an error screen showed I need java version > 11.0.10.
When using Workbench 5.4.4, if I installed a higher jdk/jre version than 1.8, it will guide me to install java 1.8. If I installed jdk/jre 1.8, it will pop up it needs 11.0.10.
When using workbench 5.4.6 or 5.Y.1, since it bundled jre, it will always pop up it needs 11.0.10. I checked the bundle java version, it's 1.8 .................
Currently, I can just use CubeMX 6.2.1 + MCWorkbench to generate source tree.
Please help to fix this issue or guide me how to use this.
Thanks,
Jungchu