Skip to main content
BTrem.1
Senior
Apr 21, 2020 5:18 PM UTC
Question

Installing Motor Profiler 5.4.3

My computer crashed & I needed to reinstall all my tools on another system. Both are Windows 10 64x. I can't get the Motor Profiler 5.4.3 to connect on the new system. When I try to connect I get a message it can't find the MFC100.dll. I installed the Visual C++ 2010 redistributable and got the same results after rebooting. I uninstalled the 2010 redistributable and repeated with the 2013 version. Same results. The system connects fine with the Motor Control Workbench 5.4.3.

What's the secret sauce ??

This topic has been closed for replies.

3 replies

BTrem.1
BTrem.1Author
Senior
Apr 27, 2020 3:51 AM UTC

I'll answer my own question after considerable debug.... The profiler is installed in the Program Filex(x86) folder; I think it's a 32-bit program. I installed both 32-bit and 64-bit Visual C++ 2010 Redistributable. So now mfc100.dll is available for both 32-bit & 64-bit. This seems to work now.

Laurent Ca...
Senior III
Jun 22, 2021 5:31 AM UTC

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards

GRobi.1
Visitor II
Jul 24, 2021 8:58 AM UTC

Je confirme qu’il faut utiliser une version c++ 2010, pas la version 2015-2019