cancel
Showing results for 
Search instead for 
Did you mean: 

FOC SDK 4.30 library PI regulator exported methods question

hankui zhang
Associate II
Posted on December 14, 2016 at 03:09

 I noticed the function description of the PI_GetDefaultKI and the PI_GetKI are same in FW API description. What is the difference between them?

I can't understand PI_

SetIntegralTerm. the description is so vague.

Can someone explain something , please?

thanks.

#library #foc-mdk-4.3
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards