Skip to main content
peterpeter9162
Associate
October 3, 2016
Question

FOC Library v4.3 available???

  • October 3, 2016
  • 3 replies
  • 843 views
Posted on October 03, 2016 at 17:37

I see in RN0085 that the FOC libary v4.3 is listed.  In new features for v4.3 I see AC6 workspace.  Yay! this is great for us.  We want to use the STM32 Open Development Env. as a base for all our firmware. 

Please can you give details on when will v4.3 be released?

Chris

#foc-4.3 #stm32-ode
This topic has been closed for replies.

3 replies

Gigi
ST Employee
October 11, 2016
Posted on October 11, 2016 at 09:08

Ciao the new version is not released yet, we are still in qualification phase.

In few week probably we will have it published.

Ciao

Gigi

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards