Skip to main content
CBald.1
Associate
March 30, 2020
Question

Encoder or Hall Sensor for X-NUCLEO-IHM16M1 ?

Hi everyone,

I am interested in buying a P-NUCLEO-IHM03 motor control pack but I would need to find, preferably, encoder or, at least, Hall sensors I can use with the X-NUCLEO-IHM16M1. Could someone please recommend me sensors that work fine with this board ? Thanks in advance.

This topic has been closed for replies.

5 replies

Cristiana SCARAMEL
ST Employee
March 31, 2020

​The X-NUCLEO-IHM16M1 have the J1 connector to manage the signal coming from Hall sensors or Encoder.

If you have a BLDC motor integrating the Hall sensors you can use that.

If you are using motor without integrated sensors,  we suggest to use a commutation encoders (e.g. CUI devices).

"If you feel a post has answered your question, please click ""Accept as Solution"""
Claire O.
ST Employee
April 3, 2020

Dear CBald.1,

Just one question: with the P-Nucleo-IHM03 there is already a motor provided. Do you plan to use the provided control Nucleo board + IHM16M1 with your own motor?

Thanks,

Claire

chaaalyy
Senior II
April 16, 2020

It also depends on the usecase: If you want to use a bldc for position control (servo... gimbal...), as far, as i know, you HAVE to use incremental encoders (3 lines: A/B/Z (Index)). Refer to https://www.st.com/content/ccc/resource/technical/document/application_note/group1/05/2a/5f/da/fa/91/40/f4/DM00691525/files/DM00691525.pdf/jcr:content/translations/en.DM00691525.pdf in this case.

If you just want to use speed control (6 step or foc), depending on the controller board, it´s not necessary to have any encoder.

With my previous experiences (and disappointed expectations...), when it comes to promoted boards and other stuff, it really helps, if you study the possibilities before you buy anything ;)

Laurent Ca...
Senior III
October 15, 2020

Dear @CBald.1​ 

Do you have still this problem to solve?

If not, do not hesitate to share the final solution you found.

Best regards

Laurent Ca...

Laurent Ca...
Senior III
October 26, 2020

Dear @CBald.1​ 

I guess you don't have to solve this problem anymore, therefore I consider this thread closed.

If not, feel free to reopen it by posting an answer.

Best regards

Laurent Ca...